2017-12-10 2:16 AM
Hi
i'm config evboar nucleo with CubeMX
the send data work fine but recive data with HAL_UART_RxCpltCallback
i's work one time and second time is stuck in loop and
don't reach to HAL_UART_IRQHandler(&huart1) again ;
i don't know why it's working one time( maybe is relevant to RXN flag )
thanks
static void MX_USART1_UART_Init(void)
{
huart1.Instance = USART1;
huart1.Init.BaudRate = 115200;
huart1.Init.WordLength = UART_WORDLENGTH_8B;
huart1.Init.StopBits = UART_STOPBITS_1;
huart1.Init.Parity = UART_PARITY_NONE;
huart1.Init.Mode = UART_MODE_TX_RX;
huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart1.Init.OverSampling = UART_OVERSAMPLING_16;
huart1.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
huart1.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
if (HAL_UART_Init(&huart1) != HAL_OK)
{
Error_Handler();
}
HAL_NVIC_EnableIRQ(USART1_IRQn);
}
void USART1_IRQHandler(void)
{
/* USER CODE BEGIN USART1_IRQn 0 */
/* USER CODE END USART1_IRQn 0 */
HAL_UART_IRQHandler(&huart1);
/* USER CODE BEGIN USART1_IRQn 1 */
/* USER CODE END USART1_IRQn 1 */
}
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
if(huart->Instance == USART1)
{
if(RX_Data=='*' || RX_Index>19 )RX_Index=0;
if(RX_Data !='♯')
{
RX_Buff[RX_Index++]=RX_Data;
}
else
{
Sync_RX=1;
}
HAL_UART_Receive_IT(&huart1,&RX_Data,1);
}
}
#cubemx #uart2017-12-12 5:18 AM
I would suggest (1) checking the return value of HAL_UART_Receive_IT() in HAL_UART_RxCpltCallback, (2) implement HAL_UART_ErrorCallback() to determine if an error is being generated.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.