2019-09-03 1:38 AM
Hi, I'd appreciate it if you could answer a few questions.
I try to use HAL_CAN_Recive_IT in the HAL example, but it's not automatically set up in CUBEMX. Why? And how do I use the HAL command in TRUESTUDIO?
Solved! Go to Solution.
2019-09-23 8:49 AM
Hello,
Processing functions (like HAL_CAN_Recive_IT) are not generated by STM32CubeMX: only initialization code is generated.
You have to refer to the examples provided in the relevant STM32Cube package of the device you selected.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2019-09-23 8:49 AM
Hello,
Processing functions (like HAL_CAN_Recive_IT) are not generated by STM32CubeMX: only initialization code is generated.
You have to refer to the examples provided in the relevant STM32Cube package of the device you selected.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.