2026-05-08 7:13 AM - edited 2026-05-08 7:18 AM
Hello everyone,
I'm using STM32CubeIDE 1.17.0 on Ubuntu 24.04.4 LTS.
Sometimes when I build or open a project, the IDE crashes and I get the following error message:
JVM terminated. Exit code=143
/opt/st/stm32cubeide_1.17.0//plugins/com.st.stm32cube.ide.jre.linux64_3.4.0.202409160955/jre/bin/java
-Dosgi.requiredJavaVersion=1.8
-Dosgi.instance.area.default=@user.home/STM32CubeIDE/workspace_1.17.0
-Declipse.buildId=Version 1.17.0
-DproductMaturityGrade=mm
-Djdk.http.auth.tunneling.disabledSchemes=
-XX:+UseG1GC
-XX:+UseStringDeduplication
-Xms256m
-Xmx1024m
-jar /opt/st/stm32cubeide_1.17.0//plugins/org.eclipse.equinox.launcher_1.6.600.v20231106-1826.jar
-os linux
-ws gtk
-arch x86_64
-showsplash
-launcher /opt/st/stm32cubeide_1.17.0/stm32cubeide
-name Stm32cubeide
--launcher.library /opt/st/stm32cubeide_1.17.0//plugins/org.eclipse.equinox.launcher.gtk.linux.x86_64_1.2.800.v20231003-1442/eclipse_11802.so
-startup /opt/st/stm32cubeide_1.17.0//plugins/org.eclipse.equinox.launcher_1.6.600.v20231106-1826.jar
--launcher.overrideVmargs
-exitdata 40031
-vm /opt/st/stm32cubeide_1.17.0//plugins/com.st.stm32cube.ide.jre.linux64_3.4.0.202409160955/jre/bin/java
-vmargs
-Dosgi.requiredJavaVersion=1.8
-Dosgi.instance.area.default=@user.home/STM32CubeIDE/workspace_1.17.0
-Declipse.buildId=Version 1.17.0
-DproductMaturityGrade=mm
-Djdk.http.auth.tunneling.disabledSchemes=
-XX:+UseG1GC
-XX:+UseStringDeduplication
-Xms256m
-Xmx1024m
-jar /opt/st/stm32cubeide_1.17.0//plugins/org.eclipse.equinox.launcher_1.6.600.v20231106-1826.jar
I found another post here with an almost identical message, but unfortunately it was closed with no answers.
Has anyone else experienced this on Ubuntu 24.04? Any suggestions on how to fix it?
Things I've tried so far:
Increasing Xmx to 2048m in stm32cubeide.ini
Cleaning the workspace
Starting with a fresh workspace
None of these solved the problem.
Thanks in advance for any help
Solved! Go to Solution.
2026-05-08 7:21 AM
Exit code=143 is a SIGTERM signal, so the JVM did not crash internally with a Java exception; it received a termination signal from the OS or another process and shut down.
Do you have enough processing power/RAM on your PC while building?
Version 1.17 is quite old tho, I would upgrade to 1.19 at least
2026-05-08 7:19 AM
Hello,
Please use the latest version of CubeIDE 2.1.1
2026-05-08 7:20 AM - edited 2026-05-08 7:25 AM
Hello @CaueEvangelista
STM32CubeIDE 1.17.0 is not officially supported on Ubuntu 24.04.4 LTS. The validated Linux distributions for this version are Ubuntu 22.04 LTS, Ubuntu® LTS 20.04,Fedora® 37
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-05-08 7:21 AM
Exit code=143 is a SIGTERM signal, so the JVM did not crash internally with a Java exception; it received a termination signal from the OS or another process and shut down.
Do you have enough processing power/RAM on your PC while building?
Version 1.17 is quite old tho, I would upgrade to 1.19 at least
2026-05-10 11:01 PM
Hello guys,
I wasn’t aware of how outdated the version I’m using is—it came preinstalled on my work machine. I’ll update to a newer one.
@nico23 : I had the same suspicion, so I monitored the RAM usage with htop while opening a project. The 8 GB of RAM were completely exhausted just before the crash. I’ll upgrade the memory and report back with the results.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.