2016-08-10 11:17 PM
Hey,
i'm using CubeMX to generate code. In one of the examples is an EEPROM emulation (STM32Cube_FW_F1_V1.4.0\Projects\STM32F103RB-Nucleo\Applications\EEPROM\EEPROM_Emulation) which I want to use. My Problem is that I can not find the Button in CubeMX so that the generated stm32f1xx_hal_conf.h enables the HAL_FLASH_MODULE_ENABLED define.I hope you can help me.Jens #cubemx-hal-flash2016-08-11 2:30 AM
Hi Jens,
The flash is enabled by default using CUMEMX.-Syrine-We’re moving the ST Community to a new platform to give you a better and more reliable community experience.