2025-04-22 10:02 PM
I am trying to configure my stm32l475 as a composite device combining a mass storage device and com port. I read that there should be an option in the "class for FS IP" dropdown to create a composite device, however I do not have that as an option. The only options listed are disable, audio device class, communication device class, download firmware update class, human interface class, custom human interface class, or mass storage class.
I am using STMCube IDE v. 1.18.1, and I ran the "check for updates" option to make sure everything is up to date.
Why is composite device not listed as an available option in STMCube ide?
2025-05-03 10:18 PM - edited 2025-05-03 10:19 PM
The reason that it was not listed seems to be that it is either no longer a feature or it was removed as a feature. I found opensource composite device software on GitHub that I used instead.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.