2016-12-08 3:31 AM
hi everyone. im new at stm32 and im trying to use lwip with cubemx (firmware :stm32cubef4 v1.14.0). my board is stm3241g-eval. and i investigated example projects and it works (ex. udp echo client) I created a new project with selected true board(my board is new and all jumpers at default) and my cube settings are:
SYS : systick
Eth : MII (its ok for default eval board)
Clk Conf : uisng HSE and CLK Mhz = 168
RTOS: no
LWIP : enabled
lwip :dhcp disable ( for static)
phyaddres: 1
eth global interrupt: enable and priority 5
i use clean code(i didnt add anything) for trying to get link at MX_LWIP_INIT function but it does not work. what is the problem? or what i must to control ? thx
#stm32cube #cubemx #lwip2016-12-08 4:32 AM
Dear
ismail_fatih
,Welcome to our Cummunity.
Which version of CubeMx are you using ? Check that you are using the last version of STM32CubeMx (4.18) with bug fixes and enhancements.
You'll probably want to review these documents which can help you to go further in your application.:
-
: it maybe helpful as it provides a full description of how to implement In-Application Programming (IAP) using Ethernet communication. - : LwIP TCP/IP stack demonstration for STM32F4x7 microcontrollers. - : user manual about “Developing applications on STM32Cube with LwIP TCP/IP stack�?-
: you can refer to theLwIP section.Hope this helps you.
Best Regards
-Imen-2016-12-09 7:18 AM
thx for your reply . my cube version is 4.18 and this documents cant help me i just select stm324x-g eval board @cubemx and than select dhcp disable and i write static ip , gw .. at textboxes then i generate it. after that i opened project at keil. i commented MX_GPIO_INIT function code cause the default code was locking MII . Than i download it to mcu and i started it. As you see this is absolutely clean code which was generated from cubemx. after starting the mcu my network symbol changed. bu at netif_link codes cannot take a link. the network cable is ok cause i tried example application with this cable and it works. this is some detailed question but i hope someone can help me
2016-12-13 8:59 AM
Hi ismail,
I tried to bring up a small application with LwIP only and found that I needed to change the PHY from 1 to zero in the header. You can see the detail at
2016-12-13 9:06 AM
Hi Imen,
Is there an application note for STM32F745 processors or is the one you link going to be relevant for that?
thanks,
hank
2016-12-13 9:22 AM
Hi
Barta.Hank
,Theapplication note is applicable to the other STM32 Series, which is usedas reference
STM32F4x7
for simplicity reason.Best Regards
-Imen-
2016-12-13 10:48 AM
Thnk u HankB
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.