STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1758 Views
  • 0 replies
  • 2 kudos

CUBEMX and TIM1 channel 1 PWM generation

Posted on February 08, 2017 at 13:09Hi in CUBEMX for a L476XX I would like to set up a PWM channel. In the pinout tab of cube under TIM1 I can choose between 'PWM generation ch1' and  'PWM generation ch1N'. So is it like it just switches the pin for...

[CubeMX] USB CDC library

Posted on June 03, 2015 at 11:37Hi,I've recently try to use code generated by CubeMX to prepare simple USB<->UART converter. Everything goes almost ok but inside function CDC_Control_FS(...) [usbd_cdc_if.c] in case ''CDC_SET_LINE_CODING'' inside buf...

licencje1 by Associate II
  • 2103 Views
  • 2 replies
  • 0 kudos

Resolved! STM32CubeMX and LL driver support

Posted on February 03, 2017 at 09:15Hello,I am guessing that code generation with LL drivers is not yet supported for product families such as F1 and F0, although it is a bit confusing that in New Library manager F0 drivers claim LL support from ver...

oversc0re by Associate II
  • 2043 Views
  • 3 replies
  • 0 kudos

STM32F334 Programm doen't start withoput manual reset

Posted on December 12, 2016 at 09:49Hi there,I have a set of 3 pcb's that i am testing I have written a programm that used to work on a previous versionof the pcb, and there have been minor changes between the 2 Version.The problem is that when i ru...

eg7963 by Associate III
  • 1791 Views
  • 4 replies
  • 0 kudos

Resolved! CubeMX: FreeRTOS USE_TICKLESS_IDLE

Posted on February 01, 2017 at 16:15In the last CubeMX version (4.19) the USE_TICKLESS_IDLE option is missing. This disables the configUSE_TICKLESS_IDLE flag and the low power configuration.Is it a bug? Is any workaround available?PS: I've checked t...

Resolved! How can I prevent stm32cubemx v1.18 from deleting my files from the project Src directory and the EWARM project? [Solved with 4.19]

Posted on January 11, 2017 at 18:02In an IAR/EWARM environment, when I use STM32CubeMX 4.18.0 Project/Generate Code function the program seems to correctly generate its own files but deletes user (that is, my files) from both the EWARM project and f...

STM32 CubeMX ST-LinkV2.1 : how to redirect printf

Posted on February 02, 2017 at 09:31I found several posts like http://www.openstm32.org/forumthread339, using syscalls.c, but I don't have this file in my project... I generate the code with CubeMX v4.18.0.#qt-creator #cubemx #stm32 #arm-none-eabi

L0_1.8.0 firmware download with STM32Cube?

Posted on January 27, 2017 at 10:22There seems to be a problem downloading the stm32cube_fw_l0_v180 from within the newest STM32Cube. See the attached screenshots. It seems to me it tries to unzip 'stm32cube_fw_l0_v180.zip' to a folder named 'stm32c...

Resolved! System Workbench build error new project from CubeMX

Posted on January 09, 2017 at 21:58Summary of 2 days investigations for CubeMX and System WorkbenchFor success build without errors imported project generated in CubeMX, need fix generated symbolsIn Project->Properties->C/C++ Builds->Settings->MCU G...

asergeev by Associate II
  • 3595 Views
  • 7 replies
  • 0 kudos

How to connect AnalogIn as source to DFSDM filter in CubeMX?

Posted on February 01, 2017 at 15:24Hello,In order to use DFSDM as lowpassfilter for my potentiometers I would like to route the ADC raw values to the DFSDM and finally get the results by DMA..Is CubeMX the right tool to prepare that? If yes, where ...

bert ro by Associate
  • 572 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.