STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

cubemx font on high res displays unusable

Posted on August 03, 2016 at 19:57Hi,Recently acquired a laptop with a 3240 x 2160 display running Windows 10.  Some of the dialog boxes and configuration tables are unusable because the fonts used do not fit within the space allocated for the text....

STM32CubeMX V4.21.0 and Java 1.8.0_131 crash

Posted on June 20, 2017 at 17:49Since my last update of WIN10, Java and STM32CubeMX (I did all after Windows update) my STM32 Cube MX crashed on lot of actions : can not load a project, can not save project etc... Any suggestion ? My PC runs WIN10 6...

Vu TRAN by Associate II
  • 4375 Views
  • 5 replies
  • 0 kudos

Uses FreeRTOS functions checkbox in CubeMx

Posted on July 13, 2017 at 10:03Hello there,I am using CubeMx with FreeRTOS for a while now. I am still not sure how does the checkbox ''Uses FreeRTOS functions'' works under NVIC Configuration settings:I would appreciate an explanation on what does...

0690X00000607WyQAI.png

cubemx modify the project properties problem

Posted on April 08, 2017 at 11:03Hi. I'm using STM32CubeMX V4.20.1 and System Workbench for STM32(SW4STM32) now.Actually I use CubeMX plugin for SW4STM32.the problem is...when I click 'Generate Code' after changing the gpios or timers or any changes...

Jisu Kim by Associate II
  • 3485 Views
  • 5 replies
  • 0 kudos

STM32CubeMX USART Limitation/Bug Report

Posted on July 06, 2017 at 19:06Hi. I have noticed that STM32CubeMX has some limitations when configuring a USART for synchronous mode. I am using a STM32F413RGTx running at 100 MHz.I am configuring USART3 for synchronous transmit/receive (pseudo SP...

Resolved! USBD_CDC_INTERVAL not used

Posted on December 06, 2016 at 18:20The define USBD_CDC_INTERVAL in usbd_conf.h generated with CubeMX is not used anywhere in the project. It was used in the old USB Library in the usbd_cdc_core.c SOF-Function, which no longer exists.#f4 #usb #cubem...

CubeMX code for Nucleo32 L432KC does not build

Posted on July 04, 2017 at 18:33Repro steps... Create a new CubeMX project, selecting the Nucleo32 L432KC board.In settings give it a name and select to generate code for the 'System Workbench for STM32' selecting SW4STM32Generate the code and open...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.