STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1759 Views
  • 0 replies
  • 2 kudos

freertos.c uses undefined __weak attribute

Posted on June 25, 2017 at 23:49I am using STM32CubeMX 4.21.0 for STM32L4.  When using FreeRTOS with tickless support, the freertos.c file is generated with functions decleared __weak, but this macro is not defined.  I am generating for GCC.  I am r...

Resolved! Encoder mode with CubeMX

Posted on April 06, 2018 at 21:47Now that encoder mode seems to be missing from CubeMX, at least for STM32F070 and STM32F407 devices, what is the most 'CubeMX-friendly' way to use it? The idea is to generate a CubeMX project, then run a script to ma...

STM32 NUCLEO-L476RG OPAMP Output not below 1.4 V

Posted on March 26, 2018 at 17:00Hey guys,i am right now working on the Nucleo L476 RG Board. I generated source code with STM32CubeMX (v4.25). I am using the internal opamp in 'Follower' mode and reading the output with the on-board adc. VCC is 3.3...

cyancali by Associate III
  • 4982 Views
  • 3 replies
  • 0 kudos

Cubemx remove unnecessarylibraries

Posted on April 05, 2018 at 19:40I created a new project with cubemx. MCU's has 8 KB flash and cubemx fulfill the code space with unnecessary libraries. How to remove unnecessary libraries from my project?#cubemx

STM32f4 + CubeMx + LwIP

Posted on April 04, 2018 at 15:31Hello,       I want to use LwIP in server mode. After a client has connected, I want to send data periodically to the client.        My device, 'STM32F4' is the server and the PC is the client.       By using the 'tc...

CubeMX v4.25 ADC config bug

Posted on March 29, 2018 at 22:28There is a bug in CubeMX version 4.25 in ADC configuration. I'm using STM32F746 MCU. In ADC2 configuration window there is one more rank displayed than number of conversion and for ADC3 there is one less. In generate...

0690X0000060AJcQAM.png 0690X0000060AJlQAM.png

STM32CubeMX warning ignoration

Posted on March 13, 2017 at 14:18Hi all,can I ask you how to turn on ignoring warning windows of STM32CubeMX.I am using it by command line interface:java -jar STM32CubeMX.exe -q <script name>I need to ignore it because my automatic build server cann...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.