STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

STM32CubeMX expansion software

Hello, I'm trying to install X-Cube PLC1 software in CubeMX by Help->Manage Embedded Software Package ->From Local >en.x-cube-plc1.zip without success!Does anyone know if this is the correct procedure? I test X Nucleo PLC 01A1 by mbed and it works, b...

STM32CubeMX with STM32F100RCT: I2C Memory with DMA issues

Hi All, I am using STM32CubeMX HAL functions (STM32CubeF1 FW package V1.6.1 in STM32F100RCT MCU project) to handle 24LC128 I2C EEPROM comms. Followed the advice in the HAL library help:DMA mode IO MEM operation:Write an amount of data in no-blocking ...

0690X000006CFGCQA4.png 0690X000006CFGHQA4.png 0690X000006CFTkQAO.png 0690X000006CFTpQAO.jpg

What freeRTOS kernel is planned for STM32cubeMX?

I am working on a project using the STM32L476, freeRTOS, and am generating code using STM32CubeMX. My team has been happy to use freeRTOS kernel v9, which has been included with STM32CubeMX so far.However, I recently updated to STM32CubeMX version ...

adamj537 by Associate
  • 1144 Views
  • 2 replies
  • 0 kudos

Resolved! Bug: CubeMX TIM3 initialisation code causes lockup

Posted on March 14, 2018 at 08:07When the attached ioc file (minimal test case, consistently reproducible) is generated using CubeMX 4.24, firmware package V1.6.0 and built with TrueStudio 9.0.0 the processor locks up when it reaches the call to __H...

Problem with PLLCLK in STM32CubeMX

Hi, I am programming STM32F051R8TX controller using STM32Cube auto-generated code. The HSI clock for the controller is 8 Mhz which can be PLL’d to 48 Mhz. When I was using the discovery board (which has the same controller) the PLL was by default set...

PR.19 by Associate II
  • 2790 Views
  • 4 replies
  • 0 kudos

Board specific pinout configuration conflict resolver

Is there a way to set the mcu pinouts based on constraints imposed by the physical wiring of the board?[Gui extension]I'm dreaming of having the ability to add custom "rectangles" and "lines" to the pinout view which represent the wiring on the board...

mcuser by Associate
  • 847 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.