STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1757 Views
  • 0 replies
  • 2 kudos

How to use i2c functions with stm32f401RE?

Hi, I'm using stm32f401RE and making a code with cubeMX.So I set i2c3 and I was going to get some numbers from LSM303DLHC whic is accelo/gyro sensor.Here's the codes what I set.​#define Slave_addr (0x1E<<1)#define X_high 0x03#define X_low 0x04uint8_t...

dlee.0 by Associate II
  • 1376 Views
  • 1 replies
  • 0 kudos

Linked directories and CubeMX code generation

I've been using CubeMX 4.12.0, and I wonder why does the code generation mess up the linked directories? Can something be done about it?The generation adds "25"s in the path, like:$%25257BPARENT-2-PROJECT_LOC%25257D/cmnThat doesn't work, but :$%7BPAR...

Where is the scrollbar?

Hello!There is no scrollbar in the windowEdit pins is practically inconceivablep.s. New design of the app is terrible (((

sstar.5 by Associate
  • 878 Views
  • 0 replies
  • 0 kudos

STM32F1 Cube MX with CAN stuff error

Hi,I tried a simple example today with STM32 Nucleo F103RB and CAN. I only generate Code with CubeMX. I do not add any line. I get a stuff error on my peak CAN if I change the "ProjectManager.CompilerOptimize=6" to "ProjectManager.CompilerOptimize=0"...

Can't download STM32CubeMX from st.com

It seems that I can't download anything from st.com. I have just clicked the download button, but nothing happend. What's going on? Is some issue on st.com or others?

Rock Deng by Associate III
  • 1790 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.