2019-01-16 7:49 AM
When USART's "Overrun" is set as Enabled (the default):
Cube generates a call to LL_USART_DisableOverrunDetect for STM32L0
Cube doesn't generate any code concerning the overrun for STM32L4
When I set "Overrun" as Disabled:
Cube generates a call to LL_USART_EnableOverrunDetect for both STM32L0 and STM32L4.
I see two issues here - the reversed logic, and a bug (difference between L0 and L4).
2019-01-16 11:24 PM
Forgot to mention that this is about the LL driver, and by reversed logic I mean enabling the "Overrun" option Cube generates Disabling code (if it generates at all), and vice versa.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.