STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Interrupt priority with Freertos

Hello,I have made a project with FreeRTOS 10.0.1.However there is a problem: when I try to call a function with ‘ISR’ suffix from interrupt service routine the macros configASSERT catches mismatch between priority that ISR has and priority that is pe...

Uhv by Associate II
  • 9384 Views
  • 8 replies
  • 0 kudos

STM32CubeMX Porting Issues

I have a project I've migrated from the STM32F407 to the STM32F405. I started by creating a new project in STM32CubeMX with the STM32F405 selected, importing my existing project, and updating the pin assignments. I was able to regenerate the project ...

BPaik by Senior
  • 809 Views
  • 0 replies
  • 0 kudos

CubeMX 5 ErrorHandler in USB CDC is called too often

Hello All,I updated to CubeMX 5 and use STM32F4 USB CDC.After update my programm crashes directly after init.This is because the USB driver calles directly into ErrorHandler when USB is not connected.The ErrorHandler does a while(1) forever loop.Why ...

taraben by Senior
  • 1666 Views
  • 2 replies
  • 0 kudos

Resolved! Missing Pin PD2 on STM32L433RCTxP

Hey,I´m confused why i can not use Pin PD2 on Cube MX on the Nucleo Board L433RC even though it should actually exist because it exist when you select another STM32L433.Without that Pin, i can´t use SDMMC. If i select for example the STM32L433RCTx, t...

SWend by Associate II
  • 4555 Views
  • 10 replies
  • 0 kudos

STM32L476G-DISCO SPI

Hi,I am working on STM32L476G-DISCO, and I want to interface it with Arduino uisng SPI, but I found that this STM all SPI (SPI1,SPI2 and SPI3) PIN is not on I/O PIN, so how I interface it with Arduino using SPI??

RKhal.2 by Associate III
  • 1397 Views
  • 2 replies
  • 1 kudos

For the STM32F100V8T medium density device can I link TIM2 (master) to TIM15 (slave) using the internal trigger ITR0?

This seems to work fine (timer linkage used in my current firmware) but the Reference manual (Doc ID16188 Rev 5) suggests this internal trigger (ITR0) is not available in low & medium density devices?! Can I rely on all future batches of the STM32F10...

0690X000008A8WtQAK.jpg 0690X000008A8YQQA0.jpg
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.