STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Where are all the examples that came with CubeMX?

Coming from a short odyssey with CubeMX and System Workbench, I just installed STM32CubeIDE. I decided so 'cause I had quite some issues in copying projects from the examples provided in the CubeMX installation and thought STM32CubeIDE would be a com...

TLaue by Associate
  • 1469 Views
  • 2 replies
  • 0 kudos

Resolved! STM32L011 Temperature sensor calibration (Possible bug in library)

Hi all, I am trying to use internal temperature sensor on Nucleo L011K4 and using macro from LL library (__LL_ADC_CALC_TEMPERATURE_TYP_PARAMS) I get complete garbage. STM32Cube_FW_L0_V1.11.2STM32CubeMx 5.0.1LL libraries used, no HALADC is running in ...

EPopr by Associate II
  • 7482 Views
  • 10 replies
  • 0 kudos

Monitor DPI problem

Is there any workaround that I can use to solve the issue regarding the super tiny font size with the ioc editor. It is actually quite difficult to work with at the moment given my laptop screen resolution is 3000x2000.

Why .json files can not be downloaded?

I use windows 10 and stm32cubemx and when i try to start a project by choosing a board selection it shows me errors downloading *.json files (mcusdocs.json, ...)I deleted the .stmcufinder .stmcube .stm32cubemx directories but no effect!

0690X000008wL6gQAE.jpg
radikv by Associate II
  • 6245 Views
  • 6 replies
  • 0 kudos

CubeMX overrides my postbuild script

Hello There,I am using CubeMX 4.26.1.I have noticed the following bug: Apart from that each time I regenerate the project in CubeMX, my truestudio project's optimization flag gets reset (this bug exist for years now), I have just noticed recently tha...

0690X0000089EmsQAE.png 0690X0000089EriQAE.png 0690X0000089ErnQAE.png

CubeMX 5.2.0 launcher broken on macOS 10.12

For some reason after the 5.2.0 update, CubeMX refuses to launch from the Finder:> You have macOS 10.12.6. The application requires macOS 10.13 or later.which is obviously not correct since I can still run this very application from the terminal just...

DEgge by Associate
  • 2063 Views
  • 3 replies
  • 0 kudos

CubeMX 5.2.0 does not load customerfirmwarePackage.

I open a project in CubeMX and specify not to use Default Firmware location and set the customer firmware location. I save the project and close the IDE. When opening the .ioc file in a text editor everything seems fine.When I open the project in Cub...

kold by Associate II
  • 1187 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.