2019-05-27 3:09 AM
I open a project in CubeMX and specify not to use Default Firmware location and set the customer firmware location.
I save the project and close the IDE. When opening the .ioc file in a text editor everything seems fine.
When I open the project in CubeMX again it has switched back to using the default firmware location.
2019-05-27 3:36 AM
Hello @DK.6old
Thank you for the feedback , issue will be fixed in the next CubeMX release.
Best Regards,
Khouloud.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.