STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1757 Views
  • 0 replies
  • 2 kudos

Resolved! STM32L462CE FreeRTOS not running

I have generated code from CubeMX for STM32L462CE controller for using the RTOS but it is not working as expected. I attached the CubeMX file. Is there any setting missed in CubemX? Please help me.

AP_040 by Senior
  • 3735 Views
  • 11 replies
  • 0 kudos

How to change "Project Location"

I have just installed CubeMX 5.2.0, and opened an saved Cube .ioc file. When I go to Project Manager the path to "Project Location" seems to be fixed to <Cube Project dir>/<Project name>I've uninstalled Cube, deleted all directories and files related...

MWebj by Associate III
  • 3817 Views
  • 2 replies
  • 0 kudos

Resolved! PWM output on Timer3 Ch1

I've my LCD backlight control on STM32F429 pin PB4, and as a digital output it was fine. I chose this pin because it can be configured as a PWM output.I've set up TIM3 Ch1 in CubeMX. I just want a free-running PWM with a dynamically configurable duty...

Resolved! STM32CubeMx can't load project - freeze

hi.When I try to open the project file, it does not respond and it does not go any further.Perhaps this is happening since the update.​attaching debug information, please confirm.​​

HJung.6 by Associate II
  • 1731 Views
  • 2 replies
  • 0 kudos

Upgrade issues from 4.27 to 5.2

We have been having issued with printf redirection on more recent Cube versions, so I got out on eval board and built a Hello World project.I created it with CubeMX 4.27, got it working (seems ?default? libraries at some point, as I had to change __i...

STM32F407VGTx / CDC / Error Driver

Hello,I test the CDC with my STM32F407VgTx in an up-to-date environment: Windows 10 / STM32CubeMx v5.20 / SW4STM32 / System WorkBench for STM32/ST-LINK V2The VCP v 1.50 driver for windows 10 has been installed normally and declared active.The source ...

CC_ROB by Associate II
  • 23990 Views
  • 29 replies
  • 0 kudos

Resolved! NVIC PRIO BITS could not be resolved - [Solved]

Hi to everybody, I am a total mcu beginner and I cannot compile a project. I did not write a single line of code, just tried to build. When I tried to do it I had 12 identical errors.What can I do? I have a STM32 F446RE Nucleo 64 board, Cube MX 5.1.0...

0690X000008wTJnQAM.jpg
AMoro.4 by Associate II
  • 3209 Views
  • 5 replies
  • 0 kudos

stm32f407 virtual com

on the win10, the stm32cubemx generated project does not work, i do not know what's the errorint main(void) { /* USER CODE BEGIN 1 */   /* USER CODE END 1 */   /* MCU Configuration--------------------------------------------------------*/   ...

0690X000008a7eMQAQ.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.