STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

bxCAN acceptance filter configuration.

Hi,I'm using CubeMX to init CAN module, everything is working, I can send and receive messages.Now I would like to configure filter to accept only message with specified ID.So, I have this piece of code generated by CUBE: //sFilterConfig.FilterNumber...

DKarc by Associate II
  • 1500 Views
  • 1 replies
  • 0 kudos

Resolved! How do I generate a BSP that CubeMX will recognize?

The FatFS library references a BSP function to determine if a SD card is plugged in. Since I don't have a BSP for this PCB, CubeMX complains about the missing function. How do I generate a BSP that CubeMX will recognize to eliminate this configurat...

GJohn by Associate II
  • 1522 Views
  • 2 replies
  • 0 kudos

STM32L452 usb support in IDE generation?

Hi.I am trying to add usb CDC to a project for the STM32L452 mcu. Project can be created, compiled without problem.I did a test with a simple and non-modified project that just had the usb added. To my despair, machines do not see the device and no e...

Resolved! HAL CubeMX I2C START problem.

-----I FOUND THE ANSWER MYSELF. ----------Technical environment :-       Master : STM32F767-       Slave : M24256 EEPROM on custom board. SCL and SDA on PH4 and PH5 with 4.7K pull-ups-       CubeMX : V5.3.0-       Normal transaction is : MASTER do a ...

I have a completed design in software via STM32Cube and SW4STM32. I need to change a PIN in CubeMX. What will happen with my finished code when I GENERATE CODE within MX with the new single PIN change?

I have completed a design using STM32F303RE Nucleo-64 board. Using STM32CubeMX and SW4STM32 (IDE). My design is done, I have build the design and there are no errors. Now I'm ready to physically download and test the design. I realize one of the PINS...

TFlac by Associate III
  • 1005 Views
  • 2 replies
  • 1 kudos

CubeMX 5.3.0 updater won't install any packeges.

I have a fresh installation of Windows 10 pro, so I need to install other things for STM, such as CubeMX. I downloaded from the site ver. 5.3.0 - installation was normal, but when I want to install FW packages for individual MCU series, I can't.Somet...

0690X00000AQm35QAD.png
pwisn by Associate II
  • 5601 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.