2019-08-21 2:40 AM
if (HAL_DAC_Start(&hdac4, DAC_CHANNEL_1))
{
/* DAC conversion start error */
Error_Handler();
}
if (HAL_OPAMP_Start(&hopamp4) != HAL_OK)
{
/* OPAMP start error */
Error_Handler();
}
HAL_TIM_Base_Start(&htim7);
// while(1)
// HAL_DAC_SetValue(&hdac4, DAC_CHANNEL_1, DAC_ALIGN_12B_R, Dacbuffers[0][0]);
if (HAL_DAC_Start_DMA(&hdac4, DAC_CHANNEL_1,(uint32_t *) Dacbuffers[0], DAC_BUFFER_SIZE, DAC_ALIGN_12B_R) != HAL_OK)
{
/* DAC conversion start error */
Error_Handler();
}Project is Cubemx generated. Everything works fine without DMA and i get result on DAC output. Trying to start DMA immediately stops with calling HAL_DAC_ErrorCallbackCh1. What can be the reason for this?
Cubemx generated code
DAC_HandleTypeDef hdac4;
DMA_HandleTypeDef hdma_dac4_ch1;
/* DAC4 init function */
void MX_DAC4_Init(void)
{
DAC_ChannelConfTypeDef sConfig = {0};
/** DAC Initialization
*/
hdac4.Instance = DAC4;
if (HAL_DAC_Init(&hdac4) != HAL_OK)
{
Error_Handler();
}
/** DAC channel OUT1 config
*/
sConfig.DAC_HighFrequency = DAC_HIGH_FREQUENCY_INTERFACE_MODE_AUTOMATIC;
sConfig.DAC_DMADoubleDataMode = DISABLE;
sConfig.DAC_SignedFormat = DISABLE;
sConfig.DAC_SampleAndHold = DAC_SAMPLEANDHOLD_DISABLE;
sConfig.DAC_Trigger = DAC_TRIGGER_T7_TRGO;
sConfig.DAC_Trigger2 = DAC_TRIGGER_NONE;
sConfig.DAC_OutputBuffer = DAC_OUTPUTBUFFER_DISABLE;
sConfig.DAC_ConnectOnChipPeripheral = DAC_CHIPCONNECT_ENABLE;
sConfig.DAC_UserTrimming = DAC_TRIMMING_FACTORY;
if (HAL_DAC_ConfigChannel(&hdac4, &sConfig, DAC_CHANNEL_1) != HAL_OK)
{
Error_Handler();
}
}
void HAL_DAC_MspInit(DAC_HandleTypeDef* dacHandle)
{
if(dacHandle->Instance==DAC4)
{
/* USER CODE BEGIN DAC4_MspInit 0 */
/* USER CODE END DAC4_MspInit 0 */
/* DAC4 clock enable */
__HAL_RCC_DAC4_CLK_ENABLE();
/* DAC4 DMA Init */
/* DAC4_CH1 Init */
hdma_dac4_ch1.Instance = DMA2_Channel1;
hdma_dac4_ch1.Init.Request = DMA_REQUEST_DAC4_CHANNEL1;
hdma_dac4_ch1.Init.Direction = DMA_MEMORY_TO_PERIPH;
hdma_dac4_ch1.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_dac4_ch1.Init.MemInc = DMA_MINC_ENABLE;
hdma_dac4_ch1.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD;
hdma_dac4_ch1.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD;
hdma_dac4_ch1.Init.Mode = DMA_CIRCULAR;
hdma_dac4_ch1.Init.Priority = DMA_PRIORITY_VERY_HIGH;
if (HAL_DMA_Init(&hdma_dac4_ch1) != HAL_OK)
{
Error_Handler();
}
__HAL_LINKDMA(dacHandle,DMA_Handle1,hdma_dac4_ch1);
/* USER CODE BEGIN DAC4_MspInit 1 */
/* USER CODE END DAC4_MspInit 1 */
}
}
Solved! Go to Solution.
2019-09-06 10:40 PM
Yes I've found the answer. You need to select destination size as 32 bit despite your source is 16 bit. DMA will do unpacking for you so
hdma_dac4_ch1.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD; // must be replaced with DMA_PDATAALIGN_WORD
hdma_dac4_ch1.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD;
Not sure if your case is the same though....
2019-08-21 2:51 AM
Hi,
do you initialise DMA before ?
This is not righ => (uint32_t *) Dacbuffers[0]
Remplace by simply (uint32_t *) Dacbuffers, or at least (uint32_t *) &Dacbuffers[0]
2019-08-21 3:38 AM
Sorry to confuse you
Dacbuffers[2][DAC_BUFFER_SIZE] Supposed to be double buffer
What do you mean by initialization. Typically cubemex do this for you (second snippet)
2019-08-21 4:39 AM
OK for Dacbuffers[2][DAC_BUFFER_SIZE]
Yes normally CubeMx generate for you a function call MX_DMA_Init() witch enable Irq and clk, but as I can't see this on your code I ask.
Do you configure the pin as analog.
You can try to you place breakpoint on DAC Irq and follow until HAL_DAC_ErrorCallbackCh1 to see what's going wrong.
2019-08-21 4:41 PM
Sure it is generated
void MX_DMA_Init(void)
{
/* DMA controller clock enable */
__HAL_RCC_DMAMUX1_CLK_ENABLE();
__HAL_RCC_DMA2_CLK_ENABLE();
__HAL_RCC_DMA1_CLK_ENABLE();
/* DMA interrupt init */
/* DMA1_Channel1_IRQn interrupt configuration */
NVIC_SetPriority(DMA1_Channel1_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(),5, 0));
NVIC_EnableIRQ(DMA1_Channel1_IRQn);
/* DMA1_Channel2_IRQn interrupt configuration */
NVIC_SetPriority(DMA1_Channel2_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(),5, 0));
NVIC_EnableIRQ(DMA1_Channel2_IRQn);
/* DMA1_Channel3_IRQn interrupt configuration */
NVIC_SetPriority(DMA1_Channel3_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(),5, 0));
NVIC_EnableIRQ(DMA1_Channel3_IRQn);
/* DMA1_Channel4_IRQn interrupt configuration */
NVIC_SetPriority(DMA1_Channel4_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(),5, 0));
NVIC_EnableIRQ(DMA1_Channel4_IRQn);
/* DMA2_Channel1_IRQn interrupt configuration */
HAL_NVIC_SetPriority(DMA2_Channel1_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(DMA2_Channel1_IRQn);
}Pin is configured correctly. It is high speed DAC and output is through built-in op-amp as follower. See CUBEMX file attached.
And everything is working including DAC output without dma.
2019-09-06 8:57 AM
I'm curious if you found and answer. I have pretty much the same problem. I notice the DMAUDRx bit gets set immediately after I turn on the timer associated with the DAC channel. Which means the data is triggered too fast. For my application it is way under 1Msps.
2019-09-06 10:40 PM
Yes I've found the answer. You need to select destination size as 32 bit despite your source is 16 bit. DMA will do unpacking for you so
hdma_dac4_ch1.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD; // must be replaced with DMA_PDATAALIGN_WORD
hdma_dac4_ch1.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD;
Not sure if your case is the same though....
2019-09-07 4:31 AM
Yes that was the issue. Thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.