STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

USB Mass storage class + SPI

I've been working with USB Mass Storage Class to create an SD Card reader with STM32L1 using SPI. I added the SDCard_SPI library and filled the missing functions in the "usbd_storage_if.c" file.What I've got is that my project works fine with SD Card...

TKou by Associate II
  • 1738 Views
  • 2 replies
  • 0 kudos

Can't enable RTOS support for USB HS

Hello, I'm using Discovery board for STM32H747XIHx, STM32CubeMX 5.5.0 and so far I wasn't able to find a way how to enable support for RTOS in USB_HOST_M7 menu in CubeMX. There is only "Disable" and it's missing "Enable". I'm not sure if I setup some...

PHlin.1 by Associate III
  • 1745 Views
  • 4 replies
  • 0 kudos

CubeMX makes error in generating Project for ARM Keilv5

Hello all!When generating a project for ARM Keilv5 with CubeMX Version 5.1.0, the file system_stm32f4xx.c ist added twice to the project under Drivers/CMSIS heading. This leads to Keil compiling the file twice and results in linker errors as some sym...

herbert by Associate III
  • 1231 Views
  • 2 replies
  • 0 kudos

EXTI_InitTypeDef and NVIC_InitTypeDef not recognized.

I set up several pins as EXTI in the CubeMX configurator, but STM32CubeIDE doesn't recognize the EXTI_InitTypeDef and NVIC_InitTypeDef datatypes. Based on the configuration I would expect the correct libraries to be included, but when compiling I get...

MAkke by Associate III
  • 2767 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.