STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1757 Views
  • 0 replies
  • 2 kudos

I receive "undefined reference to `TP_STM32_MotionFX_Library_Init'" when adding MotionFX to an existing project in STM32CubeMX.

I have added the library but I cannot build the project because there is a call to TP_STM32_MotionFX_Library_Init in StartDefaultTask (I am using FreeRTOS and Atollic) that appears to be missing from the library.If I comment out this line, the call t...

How to run STM32CubeMX in jdk13

I install jdk13.0.2 and i have generated jre using following commandbin\jlink.exe --module-path jmods --add-modules java.desktop --output jre then i add C:\Program Files\Java\jdk-13.0.2\bin and C:\Program Files\Java\jdk-13.0.2\\jre\bin to environment...

PPeng.1 by Associate
  • 861 Views
  • 0 replies
  • 1 kudos

STM32G0 [ADC-LL]: Some bugs in stm32g0xx_ll_adc.c

I think, there are some bugs in stm32g0xx_ll_adc.c.In the function LL_ADC_REG_Init() is the statement "LL_ADC_REG_SetSequencerLength(ADCx, ADC_REG_InitStruct->SequencerLength) [line 713] outside of the parentheses. I think, it should be inside the la...

problem send byte via spi dma tx

hi I'm trying to send a byte to arduino with spi2 in circular dma tx in circular mode,at the beginning the dma starts then I don't understand why the cpucrashes in the while (1), here the code: MX_GPIO_Init(); MX_DMA_Init(); MX_SPI2_Init(); MX_USART2...

SDall by Associate II
  • 2128 Views
  • 5 replies
  • 0 kudos

Suppressing repurposed SWD pins for debug

In my project the debug pins are used for the release version but naturally I would like to debug the code. Right now I have a debug macro and using #ifndef in the middle of MX_GPIO_Init function to avoid initializing debug pins. These conditions are...

MHoss.1 by Associate III
  • 984 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.