2020-03-25 7:40 AM
I have just created a new project with the latest version of CubeMX for an STM32G030F6Px and am using the code generator to provide basic bring-up code. However the generated project does not compile.
I am using System Workbench (version 1.17.0.201812190825; all updates applied), with the SW4STM32 option set in the Project Manager. However I receive the message:
../Drivers/CMSIS/RTOS2/Template/cmsis_os.h:157:10: fatal error: cmsis_os2.h: No such file or directory
I have not enabled FREERTOS in the project settings, so I'm not sure why this is being compiled. Any ideas?!
Solved! Go to Solution.
2020-03-25 8:24 AM
I'd recommend switching to STM32CubeIDE which, despite being newer, seems a bit better supported IMO.
You could grab the file yourself and move it. Seems like the path to it is slightly different than what your error message suggests.
https://github.com/STMicroelectronics/STM32CubeG0/tree/master/Drivers/CMSIS/RTOS2/Include
2020-03-25 8:24 AM
I'd recommend switching to STM32CubeIDE which, despite being newer, seems a bit better supported IMO.
You could grab the file yourself and move it. Seems like the path to it is slightly different than what your error message suggests.
https://github.com/STMicroelectronics/STM32CubeG0/tree/master/Drivers/CMSIS/RTOS2/Include
2020-03-25 9:21 AM
Many thanks for the response - I've tried with STM32CubeIDE but with exactly the same error unfortunately.
I've tried copying the missing file, but this just leads to a chain of similar missing files (at least 8!). I've found each one and copying it to the place it was looking for it and the latest error is now:
Drivers/CMSIS/Core/Template/ARMv8-M/main_s.o:C:/Users/Angus/Dropbox/STM32 Projects/PowerFlower/Debug/../Drivers/CMSIS/Core/Template/ARMv8-M/main_s.c:40: first defined hereThere is another main() defined here (with a description of 'Secure main()') but I've no idea why!
2020-03-25 10:28 AM
TDK - thanks again for your answer. I realised I was running an old version of STM32CubeIDE (1.0) - I've updated to 1.3 and all works fine now.
Thanks again!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.