STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1758 Views
  • 0 replies
  • 2 kudos

Resolved! CubeMX you really need to get your priorities right

Hi, I recently migrated from CMSIS_V1 to CMSIS_V2 ( in STM32Cube_FW_H7_V1.7.0). That came with a significant increase in the number of defined thread priorities ~ around 56 priorities. However, CubeMX sets the FreeRTOS MAX_PRIORITIES parameter to 3...

0693W000003RVOAQA4.jpg
DOsbo by Senior
  • 2433 Views
  • 5 replies
  • 0 kudos

STM32H745x Examples from STM32CubeMX not compilable

Hello,I would like to experiment on the nucleo board with STM32H745 development kit (dual cores), butr I face some issues. I just downloaded the firmware package from CubeMX and integrated the example code with SystemWorkbench4STM32 as the project fi...

AKrue.1 by Associate II
  • 2366 Views
  • 6 replies
  • 0 kudos

Resolved! Nucleo-L433RC-P garbage from USARTs - why?

Using STM32CubeIDE to create a USART test project with default code generated, the USART is outputting garbage e.g. �)���?�+Ѵ# on a terminal (USB to PC).Yet using exactly the same default code generation process and same simple test code on two othe...

PLL input frequency DATASHEET versus CUBEMX

Hello,I have found a difference between the PLL input frequency specification between the datasheet of the L4S5 :And CUBEMX data :Datasheet limit is at 16MHz, CUBEMX limit is at 8MHz.Is there any errata sheet tht specify this difference?Thank you for...

GChat.1 by Associate
  • 1817 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.