STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Strange STM32CubeIDE and .ioc behavior

Hello,For my first project with STM32 microcontrollers I try to use STM32F769I-Discovery board with TouchGFX 4.13.0 Designer and STM32CubeIDE 1.3.0.So I first generate a project with TouchGFX, generate the code and then open the project from the dire...

DNITA.1 by Associate
  • 1312 Views
  • 1 replies
  • 0 kudos

Resolved! STM32CubeMX BUG:UNINSTALLER DOESN'T RUN

Hi everyone,I wanted to uninstall my STM32CubeMX but uninstaller didn't run. I have downloaded latest version of java.Then I tried to ran uninstaller.jar in cmd I got this error Error: Could not find or load main class com.izforge.izpack.uninstaller....

Onik by Associate II
  • 4084 Views
  • 5 replies
  • 1 kudos

SAI Interface configuration small lack

Hi all,I have noted a lack in CubeMX SAI configuration. When the interface is configured as a Master, it is only possible to set frame length to a power of two from the drop-down list. Despite when I configure it manually to 20 (I need this to implem...

DmRozhd by Associate III
  • 2931 Views
  • 8 replies
  • 0 kudos

Linking error when project resides on UNC path

OS: Windows 10IDE Version: 1.4.0My project resides one a network storage folder, accessable by //BALA/my_project.The network storage is further linked to a virtual storage device, namely B:When trying to compile the project, the linking process retur...

MSonn.1 by Associate
  • 1003 Views
  • 0 replies
  • 1 kudos

Resolved! Generic makefile using stm32cubeide

Hi All,How do I generate a generic Makefile from STM32Cube ide? Preferably for L56 series. Currently when I create a project the Makefile option under toolchains inside the cubemx is grayed out. The CubeMX is installed as part of IDE. thanks,

SKuma.14 by Associate
  • 2485 Views
  • 1 replies
  • 0 kudos

Resolved! How to install firmware patch offline

Hello,I have a STM32CubeMX installed on an offline cumputer (that cannot be changed!)I would like to install the last firmware for L0 familly, so I download:stm32cube_fw_l0_v1110.zipstm32cube_fw_l0_v1113.zip (patch only file)From local, there is no p...

ANauz.1 by Senior II
  • 3402 Views
  • 3 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.