2020-11-10 6:10 AM
Hi All,
How do I generate a generic Makefile from STM32Cube ide? Preferably for L56 series. Currently when I create a project the Makefile option under toolchains inside the cubemx is grayed out. The CubeMX is installed as part of IDE.
thanks,
Solved! Go to Solution.
2020-11-10 6:19 AM
Hello @SKuma.14
Using CubeIDE, it's not possible to change the Toolchain other than CubeIDE, please use CubeMX standalone if you need to use other Toolchain/IDE.
For L5, only EWARM, Keil and CubeIDE are supported.
Best Regards,
Khouloud
2020-11-10 6:19 AM
Hello @SKuma.14
Using CubeIDE, it's not possible to change the Toolchain other than CubeIDE, please use CubeMX standalone if you need to use other Toolchain/IDE.
For L5, only EWARM, Keil and CubeIDE are supported.
Best Regards,
Khouloud
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.