STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1757 Views
  • 0 replies
  • 2 kudos

Resolved! if i will add any peripherals in existing code , existing code is disappear. new fresh code is generated

Hi, I am using STM32CUBEIDE, project creation is simple. i modified that code and i add the more function. After i need to add another peripherals, so i use .ioc (stm32cubemx) add another peripherials , after save it ask create, when into my proje...

How to disable the FreeRTOS task generation in CubeMX?

This problem was already mentioned two years ago and was allegedly fixed in version 5.2.0 of CubeMX. It is currently impossible for me to remove the default FreeRTOS task from CubeMX (6.0.1 with a STM32 F4 MCU), even removing it from the ioc file doe...

DSchw.4 by Associate
  • 2314 Views
  • 2 replies
  • 1 kudos

MX_***_Deinit ?

Am I suffering from acute dementia, or what...I recall CubeMX used to generate Deinit counterpart for each generated MX_***_Init.Like MX_GPIO_Init() and MX_GPIO_Deinit().Is my memory playing games with me, or is that deinitialization disappeared?

Resolved! CubeMX issue in regard to Preemption Priority on Uarts

Evening,I have been working on a FreeRTOS project for the last six months and all was going well until the last STMCubeIDE & CubeMX update.Rightly or wrongly, I have been using the usarts with the below interrupt config  /* UART8 interrupt Init */  H...

NW27 by Associate III
  • 3955 Views
  • 3 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.