STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! Requesting Fix: STM32CubeMX version series 6 adds two instances of #include "stm32h7xx_hal.h" to file main.h

Dear @Khouloud ZEMMELI​ ,STM32CubeMX version series 6 adds two instances of #include "stm32h7xx_hal.h" to file main.hI am observing this behavior even with STM32CubeMX version 6.1.0I observe in \inc\main.h:Line 31: #include "stm32h7xx_hal.h"Line 32: ...

CubeMX&FreeRTOS: CubeMX keeps lowering stack size for a task

Hello,today I noticed that CubeMX is behaving strangely.It gives me warnings that he had to "fix stacksize according to changed configMINIMAL_STACK_SIZE, but the problem is that this setting is 128and I try to set task to 8192 (it has normal priorit...

bully by Senior
  • 924 Views
  • 1 replies
  • 0 kudos

STM HAL and Middleware versions

What is the proposed workflow on keeping a platform updated with the latest releases of for example HAL and middleware layers from ST? Previously the code generated from CubeMX contained a version and a date, but that seems not be in the header of th...

RVikt by Associate
  • 1749 Views
  • 3 replies
  • 0 kudos

Download X-CUBE-SBSFU issue

Please click on this button to validate your ...But the dowload did not start when i click validation button​

CALAY by Associate II
  • 2032 Views
  • 3 replies
  • 1 kudos

CubeMX code generation

​Hi!i have been using cubemx for a while now, and now i am wondering regarding the code generation. in the main file , for example ,there are user code sections. can i create more of theses sections? or must i use the generated sections only?

yuri CH by Senior
  • 961 Views
  • 1 replies
  • 0 kudos

Flash wait states / VOS & STM32CubeMX generated code

I used CubeMX (v5.0.0, H7 pack v1.3.0) to generate some initialization code for the STM32H750, with the CPU core at 200 MHz and the various peripheral clocks at 100MHz.Cube then set the core voltage to PWR_REGULATOR_VOLTAGE_SCALE3 and the flash laten...

jschloss by Associate II
  • 1886 Views
  • 1 replies
  • 1 kudos

STMCubeMX returns HTTP Access Forbidden ?

I can update and install the firmware packages ok and my Windows and AV firewalls list STM32CubeMX as allowed to access the internet. In the updater Settings I get the green tick in the Check Connection button.I've uninstalled the program and re-inst...

JMaul by Associate
  • 1752 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.