STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! Clock setting saving issue

Hi,I have configured WB55 project in CubeMX but each time I reopen it, clock config isuue is displayed. When I change SMPS clock source to HSE error dissapears and I can generate project. But onviously it is not saved since next time I open it, error...

DavH42_0-1763714793579.png DavH42_1-1763714810292.png DavH42_2-1763714820907.png
DavH42 by Associate II
  • 530 Views
  • 3 replies
  • 1 kudos

CubeMX Generated ThreadSafe/stm32_lock.h - Potential Bug

I've burned a significant amount of time tracking down an issue, so I thought I would share in the hope of helping others and maybe improving ST's provided newlib locks.(This is probably in the wrong place, please move it as required.)I'm using the T...

BCowp.1 by Associate II
  • 7802 Views
  • 7 replies
  • 13 kudos

Resolved! TIM2 Interrupt deleted when setting EXTI[9:5] interrupt

Hi all,I am using a nucleo board F412ZG with the Middelware FreeRTOS. I use only one task for now, but I will use others in future.By the way, I set TIM2 as the timer system for FreeTOS:Now I am trying to enable pin PC8 as an external interrupt in or...

Fin95_0-1763709845906.png Fin95_1-1763709938606.png Fin95_2-1763709987678.png Fin95_3-1763710041206.png
Fin95 by Associate II
  • 855 Views
  • 4 replies
  • 4 kudos

Resolved! Issue when upgrading FreeRTOS plugin

Hi!I have an issue with the upgrade process of the X-CUBE-FREERTOS plugin. It happened upgrading to 1.3.0 and to 1.3.1 as well: the list of tasks defined in CubeMX seems to be retained in the CMSIS RTOS2 tab as well as the other settings, but when re...

paolog by Senior
  • 2367 Views
  • 9 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.