STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

I2C Feature Request: Please don't hardcode OwnAddress.

Hi All,In a hardware architecture where there are multiple I2C slaves running the same code base, each slave must determine their own address. The code generated by Stm32Cube hard codes the OwnAddress so it is impossible to insert a unique address in...

DOsbo by Senior
  • 746 Views
  • 0 replies
  • 0 kudos

Resolved! Bug for generate with SUBG2 ( Middleware )

Dear ST; I found bug for generate with SUBG2. I can export file to STM32CubeIDE but it can't be use with other MCU .This photo. I can generate with STM32L010.This photo. I compile source code. I found error in middleware from ST.Thank you,Best re...

0693W000007E3CLQA0.jpg 0693W000007E3CkQAK.jpg
Gz by Senior
  • 3788 Views
  • 7 replies
  • 0 kudos

STM32-MAT/TARGET External Mode - Slow update rates

Hi,I´m trying to involve STM32 MCU´s within a rapid prototyping process using Simulink and have some problems regarding the external mode. I used code geneation and external mode with PLC´s and Simulink Desktop Real-Time so far and like the workflow ...

MKain by Associate
  • 1178 Views
  • 0 replies
  • 0 kudos

Resolved! USB Audio device on Nucleo F446-RE with CubeMX

Posted on April 14, 2017 at 22:44Tried to get this working, no success.HID is OK, virtual COM, MSD, everything works fine.Audio class is recognized as composite device only. I've connected USB DP, DM and GND only. VBUS sensing is OFF.  12 MHz extern...

Resolved! Need HELP :( A proven procedure (not trial and error) to add drivers to a core project created by MXCube.

I am designing a sensor board from scratch. It will be similar to evaluation board ..\STM32Cube\Repository\STM32Cube_FW_L4_V1.16.0\Projects\B-L475E-IOT01A.I have tried example projects, they work great. Since ST do not have .ioc files for the this bo...

0693W000007EXaIQAW.jpg 0693W000007EXtyQAG.jpg
Shaun.t by Associate III
  • 1924 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.