STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

F446 and I2C-SMBUS HAL problem

Using Cube IDE. Generated a fresh project for a stm32f446ve target.Activated with CubeMX uinder I2C a port with "SMBUS-two-wire-interface".Then, without doing nothing more i have builded the configuration and flashed to target.as soon as i start the ...

MBran.31 by Associate
  • 1986 Views
  • 1 replies
  • 0 kudos

Resolved! How to turn a non-CubeMX project into STM32CubeMX configurable?

This is 3 year old question coming back again in a hope that the way was found or newly implemented to turn any STM32 example project into the configurable one to use the advantage of STM32CubeMX tool. Again, as in the past, I don't see project confi...

eBirdman by Senior II
  • 1536 Views
  • 2 replies
  • 0 kudos

I want to use MotionAD airplane detection library for aircraft detection in our product that is based on MCU that can read uart bytes from STM32 MCU.

I want to use MotionAD airplane detection library for aircraft detection in our product that is based on MCU that can read uart bytes from STM32 MCU.After reading the documentation of MotionAD airplane detection, i am not sure how it is possible that...

MAhme.4 by Associate II
  • 1148 Views
  • 1 replies
  • 0 kudos

Difference between STM32CubeIDE v.14.0 and v1.6.0?

I'm having a bit of trouble getting STM32CubeIDE v.1.6.0 to work... v1.4.0 works well for me, but the new version hangs during debugging at MX_SDIO_SD_Init(); To be clear, it's able to connect to the board, seems to download binary fine, and then ent...

PByrn.1 by Associate
  • 1520 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.