STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! STM32C071 ADC ranking missing in CubeMx

A new question moved from this thread. Thank you a lot! But still I have many questions regarding this. Like this one: I have configured the ADC with the Temperature Channel and Vref int channel to be used with DMA. However in many examples they show...

Matthias32_0-1765548300336.png

Resolved! STM32CubeMX(6.15.0) bug for NUCLEO-H723

In the STM32CubeMX configuration interface, there are two identical options here.They can be configured into different options.After generating the code, it will be based on the configuration of the second option.  

istery_0-1757838266221.png istery_1-1757838420502.png istery_2-1757838480946.png
istery by Associate II
  • 716 Views
  • 2 replies
  • 0 kudos

stm32CubeMX not listing Documents contents on Mac Tahoe

I recently switched to Mac Tahoe 26.1 and it seems since then stm32CubeMX 6.15 is not listing the contents of my Documents folder anymore. It doesn't seem like a rights management issue sincethere were no changes to the Documents rightsthey are ident...

SloBlo by Associate II
  • 1921 Views
  • 12 replies
  • 8 kudos

cubeide 2.0 UI error

as the image, after code generate in MX, instances chooser UI's graphic resolution is broken. I cannot choose any botton and projects. please solve it.

image.png
cm_lee by Associate
  • 370 Views
  • 1 replies
  • 0 kudos

Resolved! FMC on STM32H755 data/address

Hi, may I confirm whether the STM32H755 supports only the muxed PSRAM configuration? I want to experiment something with an unmuxed connection with separate data and address. Is there a work around on this or is it an internal design that I cannot ch...

ikhwanaffan_0-1765248532878.png

Use en.x-cube-cryptolib in stm32cubemx

Posted on November 09, 2016 at 15:03Hello,as I understood, x-cube-cryptolib is a plugin for the cubemx software, isn't it?But when I run SRM32CubeMX, Version 4.17.0 and use Help->Install new libraries-> from local and select en.x-cube-cryptolib.zip,...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.