STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Incorrect code generation for UART5 of F767

I generate code for stm32f767. I use software package 1.16.0 I want to use UART5 in auto baud mode via 0x55 symbol. And USART3 the same. Why code is different?static void MX_UART5_Init(void){ /* USER CODE BEGIN UART5_Init 0 */ /* USER CODE END UART...

Resolved! STM32CubeIDE generates reproducible erroneous code for the STM32L412 Nucleo-64 using ADC1 or ADC2 after a recent update to 1.7.0

STM32CubeIDEVersion: 1.7.0Build: 10852_20210715_0634 (UTC)In AL_ADC_MspInit an erroneos line is generated after a recent update of STM32CubeIDE and has to be commented out:PeriphClkInit.AdcClockSelection = ADCCLockSelection;The following error messag...

MWest.2 by Associate
  • 3371 Views
  • 5 replies
  • 0 kudos

Does the M4 core in STM32H745 support DMA interrupts ?

Hi,In Cubemx configuration, there is no option in NVIC2 (which is an interrupt controller for M4 core) for enabling or disabling DMA global interrupt. There is an option for only the M7 core in NVIC1. Are there any ways to use DMA transfer complete o...

EOzde.1 by Associate III
  • 1448 Views
  • 1 replies
  • 1 kudos

stm32h7xx_hal_eth.c V1.9.0 interrupt handling in polling mode

Even in case of not using interrupts the Function ETH_Prepare_Tx_Descriptors() line 2993 of stm32h7xx_hal_eth.c does globally enable interrupts before it exits. I would suggest using a conditional interrupt handling there (check if enabled e.g. if ne...

JRS by Associate III
  • 1024 Views
  • 1 replies
  • 0 kudos

USB HS on H730 is temperamental, constant error_handler()

I am using the H730, with the USB High Speed enabled on my own PCB setup. On some occasions, the USB will work as expected. However, most of of the time, it would enter the Error_Handler Loop. I used the CUBEIDE and ioc gui to enable the usb hsThe tr...

RAnge.1 by Associate
  • 1400 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.