STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

STM32G4 comparator output can‘t disable the PWM outputs when I want to use the fault protection mechanism。Is there something wrong in STM32CubeIDE configuration?

I tried to do a lot of changes of configuration,but it didn’t work. when I use comparator output as FLT input pin,fault protection works,however it‘s used as FLT_Int signal,it always doesn’t work.Hope your kind help,Thanks!

0693W00000AOITxQAP.jpg 0693W00000AOITsQAP.jpg 0693W00000AOITiQAP.jpg 0693W00000AOITYQA5.jpg
lshan.1 by Associate II
  • 1693 Views
  • 1 replies
  • 0 kudos

Resolved! Is there a bug in auto-generated CubeMX code that means DMA channels are not configured correctly for UARTS in STM32F407?

CubeMX (version 6.6.1 and others) generates this code. /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_USART3_UART_Init(); MX_I2C1_Init(); MX_UART4_Init(); MX_UART5_Init(); MX_USART1_UART_Init(); MX_DMA_Init(); MX_USAR...

REdmo.1 by Associate III
  • 1668 Views
  • 2 replies
  • 0 kudos

Resolved! NUCLEO-U575ZI-Q boad - CubeMX Conflicts in default project

New to STM32. I've ordered a NUCLEO-U575ZI-Q development board and have been playing with CubeMX in preparation for board arrival. In creating a project for the board I'm starting the project using the board selector and selecting the NUCLEO-U575Z...

ShawnP by Associate III
  • 1967 Views
  • 1 replies
  • 0 kudos

Resolved! CubeMX: problem when using "user constant" for FreeRTOS parameters

Hi,I'm using CubeIDE: V1.10.1 (CubeMX v6.6.1).To configure my project in (internal) CubeMX, I have created a "user constant":Name: USER_01Value: 7In FreeFRTOS Config parameters -> LIBRARY_MAX_SYSCALL_INTERRUPT_PRIORITY,I have entered this "USER_01" W...

0693W00000UoBf0QAF.png 0693W00000UoBfFQAV.png 0693W00000UoBfjQAF.png
Syn_BE by Associate III
  • 1985 Views
  • 2 replies
  • 1 kudos

Resolved! What is the version of HAL we are using?

Hi,We have selected Firmware Package STM32Cube FW_H7 V1.9.0 from CubeMX. However, the HAL Driver source file has following line:/** * @brief STM32H7xx HAL Driver version number V1.10.0 */Are the Firmware Package and HAL Driver versions different thin...

sute by Associate III
  • 4074 Views
  • 2 replies
  • 0 kudos

SIM800L doesn't respond to AT commands.

Hi there,I'm using a stm32f401re with stm32cubemx and keil uVision5. I'm trying to interface the mcu with the gsm module. I'm sure that the module works fine. I tested it with arduino and it worked without any issues. When I try to send any AT comman...

Scusi by Associate II
  • 7556 Views
  • 9 replies
  • 0 kudos

Nucleo F207: MX_LWIP_Init() not getting executed

Hi,I am using Stm32f207 Nucleo board and generated the initialization codes with cubemx.When I run the code with MX_LWIP_Init(); it's not getting executed.Commenting it works fine.Can anyone help me out to solve this issue...

SKast.1 by Associate II
  • 1680 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.