STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! Switch from stm32f407 to stm32h753

Hi,I want to switch a project in cubemx from stm32f407 to the stm32h753. (both lqfp100in cubeMX 6.8.0 there is this pinout feature to show compatible cpus. cubeMX lists me all the variants of the stm32F4, L4 and F7 but there are no H7 listed.Is there...

Jnevi.1 by Senior
  • 4569 Views
  • 5 replies
  • 0 kudos

Resolved! When will STM32CubeMX will be up to date concerning FreeRTOS?

Hello,I'm working with:STM32CubeMX version 6.8 (last version)STM32F4 FW version 1.27.1 (last version again)And, when generating a project with FreeRTOS, the FreeRTOS version is 10.3.1This version has been released more than 3 years ago!! It is comple...

ANauz.1 by Senior II
  • 1885 Views
  • 1 replies
  • 0 kudos

Resolved! Updating LSE Drive Capability does appear to work

Hi, I recently had to update the LSE Drive Capability from "low drive" (0x00) to "medium high drive" (0x02) for an STM32U575 project. After making this change in STM32CubeMx and programming the micro with the newly generated code, I noticed the updat...

AGula.1 by Associate
  • 1590 Views
  • 1 replies
  • 0 kudos

STM32F103C8T6 + MAX30003

I'm using STM32F103C8T6 controller and I want to connect MAX30003 breakout board. Which preferences it's better to use for the best performance (STMCubeMX)? Can I communicate it with an SPI slave using the UART1 synchronous mode (configured with Cube...

MGGd.1 by Associate II
  • 1574 Views
  • 1 replies
  • 0 kudos

CMSIS with Keil

Hi, I have created a project with Keil compiler (v5.17 )and I'd like to use the CMSIS driver for SPI.When I selected CMSIS in RTE, it tells me that I need CubeMX for configuring the HAL.I used CubeMX for generating the code, but there are many errors...

LBern.5 by Associate II
  • 5467 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.