STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! I2C error codes F767ZI

I am working to get one F767ZI board (master) to send 1 byte to a second F767ZI (slave).  I'm using 4k external pull-up resistors on SDA and SCL.  I am trapping errors in the master and they are:After the following code on the master I get "Error 32"...

RPatt.11 by Associate II
  • 4653 Views
  • 5 replies
  • 3 kudos

Resolved! Purpose of HAL_FLASH_Program_IT from CubeMX on NUCLEO-F746ZG?

Hi,I was wondering what is the purpose of the API HAL_FLASH_Program_IT(..) provided by CubeMX (based on NUCLEO-F746ZG but seems to be widely the same for other MCU references..).As it allows to write a single value at a time it seems useless to attem...

Nadreoh by Associate III
  • 3016 Views
  • 3 replies
  • 1 kudos

How to access spdifrx_symb_ck

In the reference manual: https://www.st.com/resource/en/reference_manual/rm0468-stm32h723733-stm32h725735-and-stm32h730-value-line-advanced-armbased-32bit-mcus-stmicroelectronics.pdf there is a clock symbol mentioned called: spdifrx_symb_ck which is ...

etheory by Senior II
  • 3935 Views
  • 8 replies
  • 1 kudos

Resolved! FPU in STM32WLE5 ??

In the System View Description file STM32WLE5_CM4.svd it says; <fpuPresent>true</fpuPresent> But the datasheet doesn't mention any FPU, the MCU Selector on st.com has a dash "-" for FPU column , and ARM docs about Cortex-M4 says that FPU is optional....

Exception in Code Generation

Starting today, on existing .ioc file, CubeMX "suddenly" complaining that project generation had a problem. "Suddenly" refers to that I have generated code incrementally many times the last few days on the same project, and today I added "FatFS" whic...

complement or replace CubeMX?

HelloI am using CubeIde and cubeMx on a project for several years with no issues.But I am facing today a limit of CubeMx:On a STM32L431RCTx I need to have UART2_RX on PA15 and PA2 as GPIO_EXT, not as UART2_TX. CubeMX forces me to have PA2 as UART2_TX...

po221 by Senior
  • 12510 Views
  • 22 replies
  • 3 kudos

Ethernet not working with cube Mx 6.8.1

Hello All,When I am configuring the ethernet for my F207 and  F7  nucleo board in its getting stucked into startup file. and through debugging when I am pressing F5 button for many times, then its getting out from startup file and my code starts work...

lavanya by Associate III
  • 3768 Views
  • 6 replies
  • 2 kudos

Include nand library

Hello friend, how to include function in library for Nand? I configuration my microcontroller from CubeMx for Nand memory and generated code, setup is bank and etc. In open code in Keil is including nand library, but is not in library is not include ...

1.png 22.png
A.Rade.96 by Associate III
  • 2277 Views
  • 2 replies
  • 2 kudos

Resolved! Possible Configuration Issue

Hello,I am using STM32CubeIDE version 1.13.0 together with STM32CubeMX version 6.9.0-RC9 and the STM32F746IGT6 microcontroller.I am trying to use TIM2 as a 4 channel Input capture unit, each channel with it's own independent DMA . For this i have the...

dte1 by Associate
  • 2550 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.