STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

CDC_Transmit_FS function always returns USBD_BUSY

I am now trying to implement CDC-VCP connection between a PC and a STM32 board. Just my goal is a STM32 echo server.​I have done like this: ​STM32 Cube MX : USB FS endableUSB Device : CDC Enable, rx/tx buffer size as 128<-1000Clock config : USB 48MHz...

SSON.2 by Associate II
  • 10401 Views
  • 5 replies
  • 0 kudos

Resolved! STM32CUBEMX 不自动生成代码问题

第一次在论坛中请教问题,如果有不对的地方,请及时通知修改,感谢 我在使用STM32H750XBH6 ,在使用STM32CUBEMX 自动生成代码时出现了问题,DMA的初始化代码没有自动生成,在不停地测试中发现,DMA Request 选择 dma_generator0-dma_generator7、MEM2MEM , 可以生成代码,选择定时比较捕获输出通道作为请求源没有自动生成代码(例如 tim4_ch1\ch2 ,tim3_ch3\ch4),cubemx版本号6.92,希望可以得到一些解决的建...

mingmieg by Associate II
  • 4108 Views
  • 2 replies
  • 0 kudos

Resolved! STM32H5: PWM generation with DMA (classic approach)

Hello,Finally I managed to produce a three-phase PWM in classic DMA mode with the pure HAL-Lib. (Hardware: NUCLEO-H563ZI) However, within the cube produced routine, file: tim.c:void HAL_TIM_PWM_MspInit(TIM_HandleTypeDef* tim_pwmHandle) This wrong cal...

AGerth by Associate
  • 3923 Views
  • 5 replies
  • 2 kudos

Problems when migrating from 6.0.0 to 6.9.2 FreeRTOS LWIP

Hello!When I took a project on version 6.0.0 and compiled it - it works stable. After CubeIDE offered to migrate to a fresh version 6.9.2 and I agreed, I set my Driver_PHY. After that the project builds, but not working.My source data:Nucleo-F767Zhtt...

ruuch by Associate
  • 2225 Views
  • 2 replies
  • 0 kudos

Resolved! STM32G431, ADC selection

Hello All,Goodday! Iam trying to configure the STM32G431RB with Cube, getting warnings when ADC-IN selected in some of the pins, and the same warnings get cleared if selected with GPIO_Analog option too. Can anyone explain please.

KSuresh by Associate
  • 1869 Views
  • 2 replies
  • 0 kudos

Related to STM32C0 board

I have connected STM32C031C6T6 board to my device but it has not been detected for some reason, it was working fine before but not working now, I have reset it as well still no use, kindly tell me what to do. 

qw1 by Associate
  • 3010 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.