2022-09-25 12:12 AM
I am now trying to implement CDC-VCP connection between a PC and a STM32 board. Just my goal is a STM32 echo server.
I have done like this:
uint8_t CDC_Transmit_FS(uint8_t* Buf, uint16_t Len)
{
uint8_t result = USBD_OK;
/* USER CODE BEGIN 7 */
USBD_CDC_HandleTypeDef *hcdc = (USBD_CDC_HandleTypeDef*)hUsbDeviceFS.pClassData;
if (hcdc->TxState != 0){
return USBD_BUSY; //<-Always triggered
}
USBD_CDC_SetTxBuffer(&hUsbDeviceFS, Buf, Len);
result = USBD_CDC_TransmitPacket(&hUsbDeviceFS);
/* USER CODE END 7 */
return result;
}
Can anybody tell me how resolve this problem?
2022-09-25 1:02 AM
2022-09-25 2:10 AM
1. In my firmware, it calls HAL_Delay(500) before CDC_transmit(..) in while body.
So I think it is not the reason of this problem.
2. I don't understand which is ISR. Do you mean CDC_transmit cannot work in "main while body"? If so, could you tell me where can I call CDC_transmit function?
2022-09-25 4:59 AM
Basically you cannot send anything if the other party is not connected = until USB device is properly initialized AND the terminal session is open.
ISR = Interrupt Service Routine. You may use CDC_Transmit in any ISR of the same priority as USB interrupt, so, for example, you may echo the received data in CDC_Receive, which is called by USB ISR.
2022-09-25 5:40 AM
Oh I understand. I will apply it and respond in tomorrow.
2023-10-25 2:48 AM
Hello, I'm having this problem too.
I created a solution as follows;
uint8_t CDC_Transmit_FS(uint8_t* Buf, uint16_t Len)
{
uint8_t result = USBD_OK;
/* USER CODE BEGIN 7 */
USBD_CDC_HandleTypeDef *hcdc = (USBD_CDC_HandleTypeDef*)hUsbDeviceFS.pClassData;
while (hcdc->TxState != 0)
{
if(usbdata_send_cntrl==1)
{
usb_com_rst=1;
usbdata_send_cntrl=0;
break;
}
usbdata_send_cntrl++;
return USBD_BUSY;
}
USBD_CDC_SetTxBuffer(&hUsbDeviceFS, Buf, Len);
result = USBD_CDC_TransmitPacket(&hUsbDeviceFS);
USB_FlushTxFifo(USB, 0x15U);
USB_FlushRxFifo(USB);
/* USER CODE END 7 */
return result;
}
" usb_com_rst=1;" in the function The variable is processed in the main() function as follows;
if(usb_com_rst==1)
{
USBD_DeInit(&hUsbDeviceFS);
HAL_Delay(50);
MX_USB_DEVICE_Init();
usb_com_rst=2;
}
As a result, the COM port is reset and this cycle is broken and the function starts working again.
However, the COM reset process sometimes causes problems on the other side (the program running on the PC).
For this reason, I want to learn how to get out of the infinite loop without resetting COM.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.