STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1757 Views
  • 0 replies
  • 2 kudos

F407 CubeMX 1.13.1FW, timer based tick error

Posted on October 31, 2016 at 04:19I use CubeMX 4.17, F4xx firmware 1.13.1, created an automatically generated timer based hal tick funtion. I tested timer 6 and timer 10. BOTH results in tick running at 2000Hz(0.5ms per tick), but I think the corre...

kiilii by Associate
  • 2484 Views
  • 4 replies
  • 1 kudos

Questions about STM32CubeMX

我有一个问题。我写了一个私人驱动程序库。如何让它在每次生成项目时自动包含写入的 .c.h 文件?每次生成项目时打开项目目录并粘贴自己的 .c.h 文件太麻烦了。如果有办法,请与我联系,非常感谢!:grinning_face:

Hi-PWC by Associate II
  • 3157 Views
  • 4 replies
  • 0 kudos

Resolved! Example ETH connection for STM32F779I-EVAL

Good morning everyone, I was given a STM32F779I-EVAL board as a gift, I am unable to configure all the peripherals installed on the board via CubeMX. For example, I can't turn on the display or configure the ETH port.Where can I find examples to unde...

Daddi by Associate
  • 1742 Views
  • 2 replies
  • 1 kudos

Resolved! STM32CubeMX 6.10.0 doesn't copy all necessary I3C headers

Reproduction steps:Open STM32CubeIDE. “File” menu → “New” → “STM32 Project”.Switch to the “Board Selector”, and pick the NUCLEO-H503RB. Click “Next”.I've successfully reproduced this issue with the NUCLEO-H503RB and NUCLEO-H563ZI. I suspect it applie...

Resolved! Ethernet peripheral missing from STM32H5 in CubeMX

The Ethernet peripheral is missing from the STM32H5 in STM32CubeMX 6.10!It appears if the Nucleo or Discovery kit boards are selected as the starting point for a project, but if the project is started from a device selection the Ethernet peripheral i...

GaryA by Associate II
  • 3216 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.