2024-03-19 5:58 PM
我有一个问题。我写了一个私人驱动程序库。如何让它在每次生成项目时自动包含写入的 .c.h 文件?每次生成项目时打开项目目录并粘贴自己的 .c.h 文件太麻烦了。
如果有办法,请与我联系,非常感谢!:grinning_face:
2024-03-19 6:22 PM
If AI translated it properly this should answer your question:
当然,为了在每次构建项目时自动包括你的自定义 .c 和 .h 文件到STM32CubeIDE项目中,你可以遵循以下步骤:
项目配置:
包含目录:
源文件:
自动化过程:
刷新项目:
如果你使用版本控制,请记得提交你的更改,以确保你的自定义配置和包含的文件被保留。此外,如果你与他人共享项目,请检查路径和设置,确保在不同的机器上正确设置配置。
按照这些步骤,你可以自动化地将你的自定义库文件包含到你的STM32CubeIDE项目中,简化你的开发过程。
2024-03-19 6:53 PM
Sorry, perhaps you didn’t fully understand what I meant. My current work scenario involves developing in Keil after generating a project with STM32CubeMX. So, my idea is whether CubeMX could possibly implement a feature to include my personal .c and .h files into the project every time it generates one.
2024-03-19 8:23 PM
Yes, CubeMX can do this. Please see the CubeMX user manual UM1718 section 6.4.
2024-03-20 12:06 AM
Hello, I have seen your reply and also found the relevant information in the user manual. It may take some time to study it. Thank you.:grinning_face:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.