2023-12-13 4:28 AM - edited 2023-12-13 4:29 AM
Reproduction steps:
Expected outcome: the project should build cleanly.
Actual outcome: compilation fails with an error:
arm-none-eabi-gcc "../Core/Src/system_stm32h5xx.c" -mcpu=cortex-m33 -std=gnu11 -g3 -DDEBUG -DUSE_HAL_DRIVER -DSTM32H503xx -c -I../Core/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc -I../Drivers/STM32H5xx_HAL_Driver/Inc/Legacy -I../Drivers/CMSIS/Device/ST/STM32H5xx/Include -I../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Core/Src/system_stm32h5xx.d" -MT"Core/Src/system_stm32h5xx.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "Core/Src/system_stm32h5xx.o"
../Drivers/STM32H5xx_HAL_Driver/Src/stm32h5xx_util_i3c.c:20:10: fatal error: stm32h5xx_util_i3c.h: No such file or directory
20 | #include "stm32h5xx_util_i3c.h"
| ^~~~~~~~~~~~~~~~~~~~~~
compilation terminated.
If I manually copy `stm32h5xx_util_i3c.h` from the HAL driver package into `Drivers/STM32H5xx_HAL_Driver/Inc/` in the project directory, the build does complete successfully. And regenerating code from STM32CubeMX removes the file from the source tree, requiring that it be manually copied in again.
This is a regression from STM32CubeMX 6.8.0.
I'm using STM32CubeIDE version 1.14.0, build “19471_20231121_1200 (UTC)”; and STM32CubeMX version 6.10.0-RC9, build “20231120-2037 (UTC)”.
Solved! Go to Solution.
2023-12-14 4:26 AM
Hello @rbr_scoleman ,
I escalated the problem to CubeMx team in an internal ticket (ID: 168810) to take a closer look at this issue.
(PS: ID 168810 is an internal tracking number and is not accessible or usable by customers).
Thanks.
Mahmoud.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-12-14 1:15 AM
Hello @rbr_scoleman ,
First let me thank you for posting and welcome to the ST Community.
Your request is under investigation, and I will get back to you ASAP.
Thanks.
Mahmoud.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-12-14 4:26 AM
Hello @rbr_scoleman ,
I escalated the problem to CubeMx team in an internal ticket (ID: 168810) to take a closer look at this issue.
(PS: ID 168810 is an internal tracking number and is not accessible or usable by customers).
Thanks.
Mahmoud.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-12-14 4:26 AM
Thank you for the update!
2024-03-19 1:59 AM
Hello @rbr_scoleman ,
Further to this comment I want to inform that this issue was resolved and the official release of STM32CubeMX V6.11.0 is available on ST website.
You can download it through this link:
STM32CubeMX - STM32Cube initialization code generator - STMicroelectronics
Thanks.
Mahmoud.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.