STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

The CubeMX/CubeIDE login issue is resolved

Hello CubeMX/CubeIDE users.  From the time period of May 14 to May 17, 2024, some users have faced issues when connecting to the ST network while using CubeMX or CubeIDE.Some examples were issues downloading firmware packages using STM32CubeMX and ST...

stm32l010f4p6 not work with MSI clock 32.768khz

"I am setting up the clock for 32.768kHz, but when I compile and test it, it doesn't work. I place a simple counter in the while loop, but it doesn't increment."i have in the while a counter, but not increment. 

clock.JPG
jdo by Associate II
  • 2388 Views
  • 3 replies
  • 0 kudos

Resolved! True version number for the CMSIS-RTOS ("injected" by CubeMX)

Hi all!Where do I find the "true" version number for the CMSIS-RTOS code "injected" by CubeMX?While STM32CubeMX (v6.9.1) shows "2.0.0"..... the header file in my project (CMSIS_RTOS_V2/cmsis_os.h) has the following in the comment header* $Date: 10. J...

mwb_0-1715758081462.png
mwb by Associate III
  • 2000 Views
  • 1 replies
  • 1 kudos

Resolved! Stm32H562 ADC DMA

When generate code for STM32H562 with active ADC + GPDMA1, I can't see code for configuration of GPDMA1. I see only this :static void MX_GPDMA1_Init(void){ /* USER CODE BEGIN GPDMA1_Init 0 */ /* USER CODE END GPDMA1_Init 0 */ /* Peripheral clock enab...

Brussl by Associate III
  • 1772 Views
  • 1 replies
  • 0 kudos

NUCLEO-H745ZI-Q Bare Metal via STM32CubeMX

Hello,  I have a NUCLEO-H745ZI-Q  I am using it to self study a bit more at the assembly level of the CM4/CM7.   I used STM32CubeMX to create a Make Project for the MCU only i.e. not the BSP / Nucleo board. I did this so I could poke around  at the C...

STM32Cube Unsupported Version

When does a version of STM32CubeMX or STM32CubeG0 and specifically the associated drivers become Unsupported? Where is this info published? Or does the latest version automatically render the previous version Unsupported.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.