2024-05-16 1:45 AM
When generate code for STM32H562 with active ADC + GPDMA1, I can't see code for configuration of GPDMA1. I see only this :
static void MX_GPDMA1_Init(void)
{
/* USER CODE BEGIN GPDMA1_Init 0 */
/* USER CODE END GPDMA1_Init 0 */
/* Peripheral clock enable */
__HAL_RCC_GPDMA1_CLK_ENABLE();
/* GPDMA1 interrupt Init */
HAL_NVIC_SetPriority(GPDMA1_Channel0_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(GPDMA1_Channel0_IRQn);
/* USER CODE BEGIN GPDMA1_Init 1 */
/* USER CODE END GPDMA1_Init 1 */
/* USER CODE BEGIN GPDMA1_Init 2 */
/* USER CODE END GPDMA1_Init 2 */
}
This is error or I don't know where to find it ?
Solved! Go to Solution.
2024-05-16 4:59 AM
Hello @Brussl ,
The DMA configuration is done in stm32h5xx_hal_msp.c. This file is part of the Src folder of your project.
It should be part of the function "HAL_ADC_MspInit".
Please , let me know if it answers to your question.
Best regards,
Gwénolé
2024-05-16 4:59 AM
Hello @Brussl ,
The DMA configuration is done in stm32h5xx_hal_msp.c. This file is part of the Src folder of your project.
It should be part of the function "HAL_ADC_MspInit".
Please , let me know if it answers to your question.
Best regards,
Gwénolé
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.