STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1757 Views
  • 0 replies
  • 2 kudos

Resolved! STM32CubeMx Ubuntu 22.04 [ERROR]

Bom dia!Instalei o STM32CubeIDE no Ubuntu 22.04, e não consigo criar um novo projeto.Ao Iniciar o CubeMX, consigo selecionar o MCU desejado e, na sequencia, retorna a seguinte mensagem de erro:Executando o IDE via terminal, no momento do erro apresen...

LeoContini_0-1723211381344.png

Resolved! SINE WAVE DAC IN STM32CUBEMX

I have a DAC signal from an ADC (potentiometer). I have set the frequency from 0-200 Hz but when I run it when I am at 200 and the sign should still be there, the signal on the oscilloscope disappears (just a straight line). does anyone know how to f...

Pwm one cycle output

Hello, I'm using STM32F030C8 and I have created 4 PWM waveforms.I want to create PWM and stop it after one cycle.I'm thinking of how to create PWM and stop directly after one cycle.  Is there any other way? Thank you.

giwonKIM by Associate III
  • 1891 Views
  • 4 replies
  • 0 kudos

Resolved! Not getting all ADC end of conversion interrupts

I'm using the STM32L475 processor with STM32CubeMX 6.11.1.I have configured ADC1 to read two channels, an external input and the internal temperature - see configuration image in CubeMX. The code to drive the adc reading is simple:int16_t Channel;voi...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.