STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

STM32CubeMX NVIC Configuration Usability Issue

I am a long-time STM32CubeMX user (7+ years). I ran into an issue with STM32CubeMX recently while modifying an existing configuration for an STM32L4 project. This is a usability issue.In the NVIC configuration page, there are two tabs, one labeled "N...

[STM32F105R8T6] CAN2 transmit working but receive isn't

I am trying to get dual 500kbps CAN working on the STM32F105R8T6. I am using CubeMX with HAL V1.6.1. CAN1 receive works and CAN2 transmit works but I cannot seem to get the CAN2 Rx interrupt to trigger.I have probed the Rx pin on the transceiver (MCP...

hjm by Associate II
  • 2450 Views
  • 4 replies
  • 1 kudos

Resolved! I2C DMA synchronization not triggering

Hi guys,I am trying to run a demo on STM32U083C-DK board. This demo consists of LPTIMER generating PWM that is used for synchronization of I2C read from on-board temperature sensor. Rising edge writes the addres of read and falling edge reads data. T...

dryet_0-1724843526621.png dryet_1-1724843567189.png dryet_2-1724843593231.png dryet_3-1724843626795.png
dryet by Associate II
  • 2469 Views
  • 4 replies
  • 0 kudos

Resolved! Updating Mbed TLS

I am considering using MbedTLS in a project. My concern is that the version in STM32CubeMX is 2.16.2 which is quite old (Jun 2019). They just released v3.0.0 last month which I believe supports TLS1.3. How long does it take for ST to update the ve...

MStra.3 by Associate III
  • 4754 Views
  • 3 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.