2024-08-15 3:26 AM
STM32CubeMX and STM32Cube_FW_H7RS_V1.1.0 has some issue, when I configure USB HS Device, the code mix some functions, such as GPIO config code etc, when I add the GPIO config it can't work either.
when the issue could be fixed??
2024-08-29 9:08 AM - edited 2024-08-29 10:53 AM
Hello @avchd,
You mean GPIO configurations code for USB_OTG_HS_DM and USB_OTG_HS_DP! This is not a bug.
GPIO configs for USB_OTG_HS_DM and USB_OTG_HS_DP are not required as they are Alternate function.
Try adding other USB pin and you will see that the GPIO config code is generated.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.