2020-08-21 1:14 AM
I would like to use the DSP. Unfortunately it already fails because of the #include "arm_math.h".
The file is not available in the project.
Is there a suitable tutorial somewhere, everything I found so far does not work.
I use a STM32F7 and STM32CubeIDE version 1.4.2.
(When creating a project the option: "copy_all_used_libraries_into_the_project" is greyed out)
2020-08-21 3:02 AM
You have to download and unpack X-CUBE-DSPDEMO software expansion. There are samples included, X-CUBE-DSPDEMO\Projects\STM32746G-Discovery\STM32F746_DSPDEMO\SW4STM32\X-CUBE-DSPDEMO builds without issues.
2020-08-21 3:22 AM
Tried it, unfortunately I could not port this into my project.
I could solve it by adding the CMSIS in the .ioc file --> Software Packs --> Select Software packs and selecting them under Software Packs --> ARM CMSIS 5.6.0
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.