2022-12-10 2:22 PM
2022-12-11 11:41 AM
Set the "Product revision" to "rev.V" and read the AN5337.
2022-12-11 12:18 AM
try just for test: use smps supply, scale 0 should be possible then.
2022-12-11 8:04 AM
nope, I tried different regulators but 0 is never in the list
main thing is that according to specs 480MHz available only with LDO but no matter what I do, I couldn’t set frequency to 480.
2022-12-11 11:41 AM
Set the "Product revision" to "rev.V" and read the AN5337.
2022-12-11 11:37 PM
REALLY APPRECIATE YOUR HELP!!!
THAT SOLVED MY ISSUE!!!
I am on NUCLEO board, playing with collecting data, lifetime is of no concern
though ST should add this to error message when I am unable to set frequency to 480 MHz
2022-12-13 12:52 AM
Hello @Pavel Krupets,
This issue is already reported in this post.
Sorry for this inconvenience.
Internal ticket number: 140578 (This is an internal tracking number and is not accessible or usable by customers).
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-03-07 12:04 AM
Hello @Pavel Krupets,
This issue has been solved in the STM32CubeMX6.8.0.
Thank you for your contribution.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.