STM32CubeMonitor (MCUs)

Ask questions on STM32CubeMonitor. Discuss the latest updates, including specialized versions (power, RF, USB-PD).

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMonitor-1.12.0 is available

Hello The version 1.12.0 of STM32CubeMonitor is available on st.com :  https://www.st.com/en/development-tools/stm32cubemonitor.html What are the main changes in this version ? Node-RED® updated to version 4.1.3.STM32 devices list updated.Software de...

STM32CubeMonitor-RF V2.19.0 is available

Hello A new release of STM32CubeMonitor-RF is available on st.com. Click on "Get latest" to download the version 2.19.0. What are the main changes in this version ? Alignment with STM32CubeWB firmware 1.24.0.Alignment with STM32CubeWBA firmware 1.8.0...

Resolved! STM32CubeMonitor v1.4.0 not acquiring on Ubuntu 20.04

I was using STM32CubeMonitor v1.30 on Ubuntu 20.04 without any problems.After upgrading to v1.4.0 my previously working flows no longer capture any data.My ST-Link V3 probe shows green on the "acq in" and "aqc out" nodes..When I click on Start Acqui...

MGieb.1 by Associate II
  • 2830 Views
  • 7 replies
  • 0 kudos

Resolved! STM32CubeMonitor-RF v2.8.1 is available

A new version of STM32CubeMonitor-RF has been released to fix some issues related to BLE OTA feature.The points covered by this release are :115533 and 117927 : During the OTA update, issue in the ACI_GAP_START_GENERAL_DISCOVERY_PROC command, change ...

Resolved! STM32CubeMonitor - validate SPI Rx buffer

I am receiving 32bit samples from an external ADC via SPI (DMA) on the STM32U5 (NUCLEO board) at a rate of 51200 samples/sec. Does the ST-Link v3e provide an interface that should allow me to reliably stream these to my PC for further anlayis/validat...

DGran.3 by Associate II
  • 3021 Views
  • 2 replies
  • 0 kudos

Resolved! [CubeMonitor] Is the log-to-csv feature broken?

I'm trying to log my data in a .csv file, using the STM32CubeMonitor v1.4.0.I'm configuring my ST processing node as follows: Sadly, it produces .csv with no data in them (see next screenshot).I also tested the same setup with the .stcm, and it worke...

0693W00000Nq7PJQAZ.png 0693W00000Nq7QgQAJ.png
GBert.2 by Senior
  • 4117 Views
  • 5 replies
  • 0 kudos

Why won't snapshot mode work for me?

I have instrumented my code as per the documentation: added dataacq.c and dataacq.h, called DumpTrace(). I do not receive any errors in STM32CubeMonitor however msg.payload.data contains only x values when I use snapshot mode. When I use direct mode ...

DGran.3 by Associate II
  • 2151 Views
  • 2 replies
  • 0 kudos

Resolved! Plotting in cube monitor

We are trying to sample a 50Hz to 200Hz signal at 50Khz rate, using stm32H7 micro controller, ADC-DMA mode is used. Tried to plot the wave in cube monitor by accessing the corresponding variable. the issue is 50Hz waveform is not reproduced properly,...

VVija.1 by Associate II
  • 11777 Views
  • 9 replies
  • 0 kudos

Resolved! Node "Single value" not working for Chart

In wiki i read about using "Single value" node for variables visualization in text frames like "Numeric" node and it working fine for it. But i cant to force to work it with "Chart" node. How it can be done?

EAlek.11 by Associate II
  • 1224 Views
  • 1 replies
  • 0 kudos

Resolved! Automatic node updating

Hello. I have "variables" node, that links to .elf file in my project in STM32CubeIDE. The project is developing now. So i want to automatically updating the node every time i build the project. How it can be done?

EAlek.11 by Associate II
  • 1236 Views
  • 1 replies
  • 0 kudos