2023-02-26 12:59 AM
Hello,
i have "splitted" the memory into several parts using the linker script.
Now i want to compile only one part to just upload that area.
They are splitted correct, so that an erase of one area will not touch the other areas.
i.e. external memory:
Area1 (r) : ORIGIN = 0x90000000, LENGTH = 2048K
Area2 (r) : ORIGIN = 0x90200000, LENGTH = 2048K
Now i just want to compile the Area2 that i have a file which only contains the Data from 0x90200000 to 0x903FFFFF
I hope that is possible.
Thank you very much.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.