STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Using STM32CubeIDE in order to program SPI1 on STM32U585AII6Q with SW NSS. The relevant pins are not initialized and PinOut seems weird.

Trying to configure SPI1 with SW NSS on STM32U585AII6Q with STM32CubeIDE.While generating the code, the relevant 4 pins are not initialized.The PinOut looks like that. This grey shade seems suspicious to me.Below, MX_SPI1_Init() and MX_GPIO_Init()sta...

0693W00000YAucvQAD.png
bmn by Associate II
  • 1819 Views
  • 1 replies
  • 0 kudos

Resolved! Nucleo-STM32f030 ADC setup Issues This code only works when I'm debugging step by step. Otherwise, it always sends ADEN low again, which should not happen!!

This code only works when I'm debugging step by step. Otherwise, it always sends ADEN low again, which should not happen!! (Correct sequence: ADEN goes high then ADRDY goes high and both stay high...) (Note both ADEN and ADRDY are low before line 54 ...

0693W00000YAXrPQAX.png 0693W00000YAXsWQAX.png
OSell.1 by Associate II
  • 4342 Views
  • 7 replies
  • 1 kudos

Resolved! What can cause HAL_ADCEx_Calibration_Start() to fail?

Here is the code snippet. HAL_Delay(5000); if (HAL_ADCEx_Calibration_Start(&hadc1,ADC_SINGLE_ENDED) != HAL_OK) { print_debug_str("Did not calibrate right!"); } else { char buf[32]; sprintf(buf,"Calibration Factor: %lu\r\n",ADC1->CA...

KiptonM by Lead
  • 12545 Views
  • 4 replies
  • 0 kudos

Resolved! I try to use pmd-eclipse plug-in (static analysis tool). Plug-in is installed and I added -vm corresponding option in stm32cubeide.ini to define correct jdk version but it still not works

The error message says that this plug in needs jdk 17 : jdk 17 is installed and I have added the option -vm with corresponding path to javaw.exe. Error Message is still present after CubeIDE restart.

DWeya.1 by Associate
  • 1236 Views
  • 1 replies
  • 0 kudos

Resolved! How would you go about adding the version and 8 characters of the git hash to the hexfile name so we can also access it in the program?

Say we have a STM32 project called Foo. When it is compiled, it generates an intel hex file called Foo.hex that we can use to upgrade the file in the field. That is easy. What we would like to do as add the version say 10.1 or 10_1 and the last 8 di...

KiptonM by Lead
  • 4509 Views
  • 4 replies
  • 0 kudos

SPL2LLConverter compatibility_api.h

Hello, I used SPL2LLConverter tool to migrate a project. The migration went fine but in some of the source files a compatibility_api.h is included which is nowhere to be found. Any clues of what is this file and if it is necessary? If it is, where ca...

PBlan.1 by Associate
  • 1360 Views
  • 1 replies
  • 0 kudos

where .ide.log file is save and can i change this folder

I import a project , in a different workspace (change folder) after i rename the project with new name, but every time i launch this project a old folders of old project is generated with inside .ide.log file of current session.What can i do to solve...

PMaro by Associate
  • 3788 Views
  • 3 replies
  • 3 kudos

Resolved! Can we create DLL file from STM32CubeIDE? Just like as in Visual Studio, one can create DLL file from C language to be used by other languages.

 I have a big project in C that was created by other people, it builds and run well on STM32CubeIDE. I want to create DLL file out of this to expose the functions used inside so that it can be used by other programming languages.

SChen.24 by Associate
  • 2190 Views
  • 1 replies
  • 0 kudos

What is the issue with the USB Custom HID Low Level Driver?

For a STM32L433CB I generated the Custom HID code using CubeMX version 6.2.1 and the Cube FW_L4 V1.17.0The CUSTOM_HID_FS_BINTERVAL   is set to 5ms and I placed a Custom HID Descriptor. Also I adjusted USBD_CUSTOMHID_OUTREPORT_BUF_SIZE and USBD_CUSTOM...

SPfis.1 by Associate II
  • 7688 Views
  • 11 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.