2025-12-10 1:36 PM - last edited on 2025-12-12 1:42 AM by Andrew Neil
Title edited to correct version number.
I have not programmed in the IDE for a while. But when I created a project, and edited the .ioc file, and told it to save and create the main.c file it did, and opened the main.c file.
I am able to create a project, and it lets me go to the MX editor (I am in 1.9.0). I enable a couple of UARTS,
Then I save. And it asks if I want to generate code, I say yes. And there is no code at all.
There are only two files in the EPS_PDU_STM32L433RCT3 project directory the
EPS_PDU_STM32L433RCT3.ioc
.project
None of the subdirectories were created, the main.c was not created.
This used to work. I must have fat fingered something to screw it up. But I do not know what I did.
I did see a warning on the project name in the Project Explorer
Description Resource Path Location Type
Project 'EPS_PDU_STM32L433RCT3' has no explicit encoding set EPS_PDU_STM32L433RCT3 /EPS_PDU_STM32L433RCT3 No explicit project encoding
I do not know what that means. I do not think I changed anything.
Is that encoding right for Linux?
It looks like it inherited UTF-8 from linux. Other is UTF-8 what is wrong?
Is this causing my issue?
I am used to seeing Core, Debug, Drivers, .settings directories in the project directory.
Also no .ld linker file and others.
But in my project directory I have only the two files mentioned earlier.
What did I screw up? How do I fix it.
Solved! Go to Solution.
2025-12-11 12:58 AM - edited 2025-12-11 12:59 AM
Hello @kmoravec
Could you check if the firmware is installed? If not, you should go to Help> Manage embedded software packages and install the missing firmware.
KR, Souhaib
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-12-11 12:58 AM - edited 2025-12-11 12:59 AM
Hello @kmoravec
Could you check if the firmware is installed? If not, you should go to Help> Manage embedded software packages and install the missing firmware.
KR, Souhaib
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-12-11 1:28 AM
Do you really mean v1.9 - that's very old !
Or do you mean v1.19 - which was the last v1.xx before the current v2.0.0
2025-12-11 10:26 AM
Yes I meant 1.19, sorry about that. People here recommended I stay with 1.19 because 2.0.0 because of the MX separation.
Thanks for the response.
Kip
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.